REGEN.TESTVTHRESH
Description
This command is used to configure the timeout expected by the regen self-test feature. See REGEN.TEST for more info on how this timeout is used.
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-07-03-000 |
|
General Information
|
Type |
Read/Write |
|
Units |
Percent (%) |
|
Range |
60 to 99 |
|
Default Value |
80 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
REGEN.TESTVTHRESH |
3007h |
0ah |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2409 |
1 |
2409 (0x969) |
REGEN.TESTVTHRESH |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REGEN.TESTVTHRESH |
2409 |
Unsigned8 |
Read/Write |
- |